Would anyone explain what is the meaning of the letter after " / "?
RD24FS-T1-AY/BW
PS2701A-1-F3-A/L
UPC393MF-DAA-E1-AT/H
UPC393G2-E2-A/H/HM
UPC844G2-E1-A/HE
UPC842G2-E1-A/HM
UPC1093T-E1-AZ/S
UPC1093T-E2-AZ/S
hmmm.. no obvious answer. I'll need to take this away and revert back to you .. BR john
quick question : where do you see these referred to ? I cannot see in datasheet or order code, so wonder if this is from a different manufacturer of these generic part numbers.
Thanks
JE_REN
What's the difference between E1 and E2? E1??E2??
Hi,
As I understand in our part code there no suffix after "/" .
Ex. UPC844G2-E1-A
...
Hi
E1 & E2 in UPC393G2-E2-A/H/HM, /UPC844G2-E1-A/HE /UPC842G2-E1-A/HM .is for pulling direction
Standard IC Part Number Guide
AB
Is the P/N of UPC1093T-E1-A the same?the difference between E1/E2 (Taping direction)
Hi ,
Yes ,
You can refer the attached guide link to understand the nomenclature
very thanks!!