How to download firmware to the EC-1 using a flash programmer?E

Hi

I want to download firmware to EC-1. But, i can't find documents related to use flash programmer with EC-1

also, Not even EC-1(Cortex-R4) on the list of MCUs supported by Renesas Flash Programmer V3

 

How can i use flash programmer with EC-1?

Or not, which of the other programmer should i use to download ?