I want to confirm if the HS9-26CLV32RH (and also the HS9-26CLV31RH) has a metal bottom. I found this in both datasheets:
Is the lead finish referring to the bottom of the component? I need to know if it will short any traces or vias underneath the component.
The lead finish shown in the package outline drawing in the datasheets is referring to the leads extending out from the package.
The bottom of these parts that would rest on the PCB are ceramic. It is non-conductive so it is ok to place traces or vias underneath the component.