HS9-26CLV32RH physical details

I want to confirm if the HS9-26CLV32RH (and also the HS9-26CLV31RH) has a metal bottom. I found this in both datasheets:

Is the lead finish referring to the bottom of the component? I need to know if it will short any traces or vias underneath the component.