ISL71840SEH VREF range

In the datasheet for the ISL71840SEH analog mux it says the range the VREF input is 4.5 to 5.5 V. However, if I were to use 3.3V for VREF, would it still work?

On page 23 it says that about 30% of VREF is what sets the logic threshold, so with 5V VREF the threshold would be about 1.5V, and with 3.3V VREF the threshold would be about 1V.

If a 1V logic threshold works for me, then can I use 3.3V for VREF, or are there other consequences of going below 4.5 V?

Parents
  • Hello Charles,

    The specification in the SMD for VIH/VIL is done with Vref = 5V.  It is saying that when VIH is ≥ 1.6V, on a logic input (A2,A1,A0, ENbar), it will be in the Hi-state.   When VIL ≤ 1.2V, on a logic input (A2,A1,A0, ENbar),  it will be in the Low-state.    Between 1.2V and 1.6V the logic stage is undetermined.  As stated in Figure 80 in the Renesas data sheet the switching point at Vref = 5V  is around 1.4V.   

    We only guarantee VIH / VIL with Vref = 5V.  All parts are tested across temperature and radiation with Vref = 5V  to ensure they meet the VIL and VIH of 1.2V and 1.6V.

    If VREF is 5V the logic control inputs will support 3.3 V logic 

    There is no specification or testing done with Vref at 3.3V. 

    We apologize but we cannot answer questions on a public forum for our space parts unless the information is already posted on our public website. In this case, the information I provided in on a public SMD.

    For any further support on this you will need to submit a Technical Support ticket by going to our support portal from the following link: https://en-support.renesas.com

    You will need to sign in with your company email address, and if you don't have an account you will need to register with one. https://www.renesas.com/register  

    Best regards, Cindy Huberty, Renesas Electronics, Online Applications Support Engineer

Reply
  • Hello Charles,

    The specification in the SMD for VIH/VIL is done with Vref = 5V.  It is saying that when VIH is ≥ 1.6V, on a logic input (A2,A1,A0, ENbar), it will be in the Hi-state.   When VIL ≤ 1.2V, on a logic input (A2,A1,A0, ENbar),  it will be in the Low-state.    Between 1.2V and 1.6V the logic stage is undetermined.  As stated in Figure 80 in the Renesas data sheet the switching point at Vref = 5V  is around 1.4V.   

    We only guarantee VIH / VIL with Vref = 5V.  All parts are tested across temperature and radiation with Vref = 5V  to ensure they meet the VIL and VIH of 1.2V and 1.6V.

    If VREF is 5V the logic control inputs will support 3.3 V logic 

    There is no specification or testing done with Vref at 3.3V. 

    We apologize but we cannot answer questions on a public forum for our space parts unless the information is already posted on our public website. In this case, the information I provided in on a public SMD.

    For any further support on this you will need to submit a Technical Support ticket by going to our support portal from the following link: https://en-support.renesas.com

    You will need to sign in with your company email address, and if you don't have an account you will need to register with one. https://www.renesas.com/register  

    Best regards, Cindy Huberty, Renesas Electronics, Online Applications Support Engineer

Children
No Data