Hi friends,
What is the frequency of the internal oscillator?.
Using internal oscillator, what is the maximum frequency that I can indicate for the SPI protocol?.
To read data from the isl26102, must the /cs be set to 1 (which is the opposite of when reading or writing to registers)?. Thanks,