Hi,
I am using DA7219 performance board for the codec. I am unable to playback using DA7219 GUI. I would like to verify USB Playback, For this, I followed this document DA7219 Readme and Quick Start.pdf. As per the document, the script is required. But when I installed GUI, I am not getting any type of script. Can you please provide me the playback supported script??
Thanks,
Divyesh
Hi Divyesh,
Thanks for reaching out. Please find attached the requested script. Let us know if you have any further question
Kind Regards
Shivani
//***************************** FILE HEADER ************************************// // // // Filename: .txt // // Author: BM // // Date: 10-Aug-15 // // Description: //******************************************************************************//
WRITE DA7219 0x13 0x80 //RESET
WRITE DA7219 0xFD 0x01 //Enable ACTIVE mode WRITE DA7219 0x13 0x01 //Enable repeat mode register access (register address and data is sent for each write) WRITE DA7219 0x91 0x01 //IO Level 1.5-2.5V WRITE DA7219 0x32 0x08 //Enable Master BIAS and VMID (VMID and Bandgap enabled on BIAS_EN)
WRITE DA7219 0x20 0x08 //PLL Disabled, PLL INDIV= 10-20MHz WRITE DA7219 0x17 0x0B //48kHz sample rate WRITE DA7219 0x2C 0xAC //DAI Enabled, DAI Channel 1L and 1R enabled, 32bit, I2S WRITE DA7219 0x2B 0x01 //Slave Mode DAI, 64xFS BCLK WRITE DA7219 0x30 0x00 //No Offset on DAI (lower) WRITE DA7219 0x31 0x00 //No Offset on DAI (upper)
WRITE DA7219 0x47 0xA0 //Enable Charge Pump DAC VOL mode WRITE DA7219 0x95 0x0E //Set CP Threshold to 0x0E WRITE DA7219 0x44 0x80 //Enable DAC HPF WRITE DA7219 0x2E 0x32 //DAC right source is DAI, DAC left source is DAI WRITE DA7219 0x3C 0x01 //No sidetone WRITE DA7219 0x3D 0x02 //No sidetone WRITE DA7219 0x4B 0x01 //MIXOUTL enabled WRITE DA7219 0x4C 0x01 //MIXOUTR enabled WRITE DA7219 0x51 0xF1 //Enable stereo DAC, MIXOUT and HP
Hi Shivani,
Thanks for your reply, I have tested playback on DA7219 EVK Module and playback works successfully.
Hello Ssaravan,I use this script and playback audio ok but can't record.Can you help me new script or some solution?
Hi ,
I will check with concern AE and come back to you
Thanks
AB