Hello,
I am using ISL79987 with i.MX 8M Mini.
I created a customized embedded Linux (Kernel 6.1.36) distribution with Yocto.
I have activated the ISL79987 Video Decoder IC.
Although the IC is 4-Channel, I see "video0", "video1", and "video2" under the "/dev" directory.
I am using the following configuration as DTS.
isl7998x_mipi@3d { compatible = "isil,isl79987"; reg = <0x3d>; ports { #address-cells = <1>; #size-cells = <0>; port@0 { reg = <0>; isl79987_out: endpoint { remote-endpoint = <&mipi_csi2_in>; data-lanes = <1>; }; }; port@1 { reg = <1>; endpoint { /*remote-endpoint = <&camera_0>;*/ }; }; port@2 { reg = <2>; endpoint { /*remote-endpoint = <&camera_1>;*/ }; }; port@3 { reg = <3>; endpoint { /*remote-endpoint = <&camera_1>;*/ }; }; port@4 { reg = <4>; endpoint { /*remote-endpoint = <&camera_1>;*/ }; }; }; };
Where am I going wrong? Could you help me with this issue?
Best regards,