Please tell me how to using about ISL79987.

Hello
I have a question about the ISL79987.
I am actually designing a circuit, but is it correct to connect VSSM, which is the GND of VDDM, to the analog ground?
My understanding is that MIPI is a digital signal, so I thought it should be connected to the digital ground, so this is my question.

Parents Reply Children
  • Dear AB

    Thank you very much for your answers.

    I understand that MIPI output signals are considered analog because analog blocks are involved.

    I also understand that all grounds should be connected.

    But I just can't understand it.

    In the diagram below, should VDDP and VDDM be classified as AGND?

    This is an excerpt from the hardware manual.

    Considering the pin layout, I would assume it is designed to be connected to DGND.