Hi all,
I am encountering several issues with the integration of the DA7219 on our platform. I have successfully configured the codec's I2C interface for proper read and write operations. Additionally, I managed to get the I2S interface working from the CPU, but I am still unable to produce any sound from the codec.
I have modified the sof_da7219_max98373 driver to align with our hardware configuration and a kernel version 6.6.56.
sof_da7219_max98373
For our platform, I am using the codec in slave mode for the PLL and the following clock settings:
Despite tracing all functions, I have not been able to properly configure the PLL or the codec registers. To address this, I attempted a fixed configuration, but I still couldn’t get any sound output from the codec.
Could you provide support with configuration tweaks or share any advice?
Best regards,Romain
Hi Romain,
I will get back to you on this query.
Thanks, and regards,
Avinash Kumar