DA7212 Initialization

Hello,

On some of our boards the DA7212 draws a high current (up to 1.5A for about 5 ms) during initialization, when the line output is enabled (register 0x6D).
This happens about 10 ms after the first I2C write and probably internal circuits are not yet correctly biased.
The datasheet only mentions a 25 ms typical start-up time for the  VMID supply in chapter 12.1.

In the example init scripts you always have a 40 ms delay after the first I2C communication.

Is this for this reason and is this always sufficient? Do we have to observe other timings during startup?
Does the SLC2 solve this timing issues automatically?

Thank you and best regards

Martin

Parents Reply Children
No Data