SLG46620G's OSC Oscillator Block Won't Generate an Internal 2 MHz Clock

I have a fairly complex design implemented in a GreenPak SLG46620G and was in the middle of debugging it, when suddenly the OSC unit stopped generating a 2 MHz clock. After hours of trying everything I could think of with no success, I created a trivial (but valid and useful) design that simply routes the OSC's OUT0 output to a pin. Even that doesn't work!

In attempt to isolate the problem, I added a simple multivibrator consisting of a "P DLY1" delay and an "INV" inverter looped together, and fed the inverter's output into OSC's CLK2 input. When this input is selected to feed the OUT0 output, the "clock" passes through successfully.

What is wrong? I hope it fails for you, so I don't have to debug some obscure problem on my PC running Windows 11.

Thanks in advance!

-- Jim

Download the file (right-click and choose "save link as...") at:

https://questrak.com/downloads/Oscillator_Test.gp4