SLG47105 rechargeable electronic screwdriver

Hello.

We are interested in using the SLG47105 to manage a DC motor.

This motor must operate in both directions, this can be selected using two switches. It is necessary that the DC motor is able to supply all the torque it can give. It would be interesting to have the integrated controller monitoring the current supplied to the motor and if it sees that it is excessive, cut the power supply.

The system should be powered by a 3.7 V lipo battery The component should also manage the load of the battery when it reaches a certain level and stop the load when it detects that it has been fully charged. 

We have seen some documents published by Renesas about this integrated with similar applications (AN-CM-364 Rechargeable Electric Screwdriver), but we need support on how to use this configuration we need.

Thank you in advance,