Question about Evaluation Environment for GreenPAK SLG47004V.

Dear all,

Hello.

I'd like to know what we shoud use for evaluate the SLG47004V.

- Can we use SLG4DVKADV with SLG47004V-SKT and SLG47004V itself for the best way to evaluate ?

- Can we use SLG47004V-EVB for the best way to evaluate ?

- Can we get the spec sheet about SLG47004V-SKT ?

- We look SLG47004V-SKT does not have connect pin no.7 and no.8. Does the board have no way to connect to external circuit about these pins ?

Parents
  • Hi, 

    I ll check on spec sheet SLG47004V-SKT   and get back to you .

    Thanks 

    AB

  • Hi, 

    Kindly find below details:-

    Q:- Can we use SLG4DVKADV with SLG47004V-SKT and SLG47004V itself for the best way to evaluate ?

    Ans:-This DVB Kits can emulation, test and re-program/burn the design to blank chips, and very easy to replace the chips.

    Q:- Can we use SLG47004V-EVB for the best way to evaluate ?

    Ans:-Work with GreenPAK Serials Debugger boawrd, this EVB Kits can emulation, test and re-program/burn the design to chips, but the chip was fixed on the board, of course, customer can add Peripheral components on the board for further evaluating.

    For the spec sheet about SLG47004V-SKT , kindly check the inbox.

    Q:- We look SLG47004V-SKT does not have connect pin no.7 and no.8. Does the board have no way to connect to external circuit about these pins ?

    Ans:-Connect pin no.7 and no.8. are tied to SV3, for more details, you can also refer to the SCH and Gerber file.

      

    Thanks

    Ab

Reply
  • Hi, 

    Kindly find below details:-

    Q:- Can we use SLG4DVKADV with SLG47004V-SKT and SLG47004V itself for the best way to evaluate ?

    Ans:-This DVB Kits can emulation, test and re-program/burn the design to blank chips, and very easy to replace the chips.

    Q:- Can we use SLG47004V-EVB for the best way to evaluate ?

    Ans:-Work with GreenPAK Serials Debugger boawrd, this EVB Kits can emulation, test and re-program/burn the design to chips, but the chip was fixed on the board, of course, customer can add Peripheral components on the board for further evaluating.

    For the spec sheet about SLG47004V-SKT , kindly check the inbox.

    Q:- We look SLG47004V-SKT does not have connect pin no.7 and no.8. Does the board have no way to connect to external circuit about these pins ?

    Ans:-Connect pin no.7 and no.8. are tied to SV3, for more details, you can also refer to the SCH and Gerber file.

      

    Thanks

    Ab

Children