I am using the Kria KV260 Starter Kit. I would like to know if there is any way of acquiring the SLG7XL44677 component or, if case it is not possible, I would like to receive the code of the reset logic or, at least, how it works more accurately. Even if we do not intend to use it in the same device, I would like to understand the reset sequence and functions. Thank you!
Xilinx have published the GreenPAK design file:
https://support.xilinx.com/s/article/000035025?language=en_US
The SLG7XL44677 is an SLG46721V. Therefore, if you have a GreenPAK programming device, you can make one yourself. Buy an SLG46721V (Mouser has them on stock), then open the .gp3 file in the Go Configure Software Hub, and program it. You can, of course, also study the logic in the Go Configure Hub.