Hello all,I am completely new to GreenPAK and want to include a SLG46108V with AN-CM-318 on a custom PCB.
How do I program the chip?Do I need to buy the SLG4DVKADV or are there cheaper options (like using a generic USB to serial adapter or some Arduino sketch)?
Are there other options to get pre programmed chips? According to the FAQ the minimum order quantity is 3000 but my requirements are ~10 pcs.
Best,
gilex
Hi,
You can understand the difference between development boards by referring to page no.5 (GreenPAK TOOLS)
GreenPAK Configurable Mixed-Signal Matrix Family Overview (renesas.com
Kindly note this is one-time (factory) programming of NVM chip .Evan though you can change the configurations, but once the chip power down, all the changes will be erased and will be reload the default configuration from NVM when next power on the chip and this chip comes STQFN-8 package .
Thanks
AB