The available options for IO0 are:
However the datasheet does not document this restriction and mentions this is GPIO: so why is Digital input/output not an available option in GreenPAK designer V6.36?
Hi,
First of all please update the designer software to latest version.
The PINs has OE terminal which indicates it can be set as Digital input/output.
Since the OE’s state decides the PIN will work as Input mode or Output mode.
Thanks
AB