Advanced Development Board stops responding

I have a new ADK board, H/W rev 1.3.1, F/W 3.4 supplied with the SLG4DVKINTRO. No updates appear to be available.

I have a simple design for SLG46826V, created using Go Configure / GreenPAK Designer V6.44. Running on Win 10, 22H2.

I'm using a slow (6s period), sine generator to one pin on the device, and a couple of emulated push button inputs.

This all works in s/w emulation.

When emulation is run on the ADB, it usually works for some time, but user input (button presses within Go Configure), causes the system to lock up.

Occasionally it will recover, but usually it requires the ADK to be disconnected from the USB port, and reconnected, before the GF IDE can gain control again.

GP designer reports "Device didn't answer - The board didn't connect within the expected timeframe.Please reconnect the board and try again."

I believe the fault does not occur if I don't run the slow sine generator.

Is this a known fault with the ADB, or with designs using the generator on the ADK? Any suggestions to avoid this fault?

Parents Reply Children
  • Hi, 

    You can share here if you okay? (but this public forum) .

    OR 

     You on this you can submit a Technical Support ticket by going to our support portal from the following link: https://en-support.renesas.com

    You will need to sign in with your company email address, and if you don't have an account you will need to register with one. https://www.renesas.com/register 

    Thanks 

    AB

  • Ok, it's a .gp6 attached with extension changed to txt. There's nothing sensitive in this file - it's just to examine the fault.

    <?xml version="1.0" encoding="UTF-8"?>
    <GPDProject version="33" oldestCompatibleVersion="32" GPDVersion="6.44.001" lastChange="5 Sep 2024 10:40:26" projectChecksumState="1" projectChecksum="c5a58951">
        <generalProjectSettings/>
        <chip family="04" type="06" friendlyName="GreenPAK 6" partNumber="36" package="7">
            <nvmData registerLenght="2048">22 3 0 3A 14 42 8E E4 3 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 30 48 E 0 F8 0 E0 3 0 0 0 0 0 0 0 0 0 0 F0 3 0 0 0 3E 0 0 E8 F 0 0 F0 FC 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 30 8 0 30 30 30 8 0 0 30 30 30 0 30 30 30 3 0 30 0 0 0 0 0 0 0 0 0 0 0 0 0 0 2 0 0 14 22 38 C 0 0 68 0 0 0 0 E8 4 0 0 70 0 0 0 0 0 14 0 0 0 0 0 0 0 0 20 0 1 0 44 E4 57 7F 10 0 E7 1 32 2 0 28 20 0 0 2 0 1 0 0 2 1 0 0 2 0 1 0 0 2 0 1 0 0 0 1 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 A5</nvmData>
            <eepromData id="0">0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0</eepromData>
            <checksum crc32="0xC0540085" version="7"/>
            <VDDItem id="0">
                <item id="0" caption="VDD (PIN 1)">
                    <graphics pos="(483.64,-315.64)" angle="0" flipping="0" hidden="0" tOrigin="(20.00,10.00)"/>
                </item>
            </VDDItem>
            <IOPad id="1" useCaseMode="0">
                <item id="1" caption="PIN 2 (IO0)">
                    <graphics pos="(792.13,-513.05)" angle="180" flipping="0" hidden="0" tOrigin="(20.00,10.00)"/>
                </item>
            </IOPad>
            <IOPad id="2" useCaseMode="2">
                <item id="2" caption="PIN 3 (IO1)">
                    <graphics pos="(786.49,-14.00)" angle="0" flipping="1" hidden="0" tOrigin="(20.00,10.00)"/>
                    <textLabel pos="(5.50,-27.00)" angle="0.00" textColor="#ffff00ff" backgroundColor="#14141464">led1</textLabel>
                </item>
            </IOPad>
            <IOPad id="3" useCaseMode="1">
                <item id="3" caption="PIN 4 (IO2)">
                    <graphics pos="(-130.08,105.94)" angle="0" flipping="0" hidden="0" tOrigin="(20.00,10.00)"/>
                    <textLabel pos="(2.00,-27.00)" angle="0.00" textColor="#ffff00ff" backgroundColor="#14141464">mode</textLabel>
                </item>
            </IOPad>
            <IOPad id="4" useCaseMode="0">
                <item id="4" caption="PIN 5 (IO3)">
                    <graphics pos="(667.06,-474.74)" angle="180" flipping="0" hidden="0" tOrigin="(20.00,10.00)"/>
                </item>
            </IOPad>
            <IOPad id="5" useCaseMode="0">
                <item id="5" caption="PIN 6 (IO4)">
                    <graphics pos="(663.66,-514.35)" angle="180" flipping="0" hidden="0" tOrigin="(20.00,10.00)"/>
                </item>
            </IOPad>
            <IOPad id="6" useCaseMode="2">
                <item id="6" caption="PIN 7 (IO5)">
                    <graphics pos="(782.42,223.26)" angle="180" flipping="2" hidden="0" tOrigin="(20.00,10.00)"/>
                    <textLabel pos="(34.50,47.00)" angle="-180.00" textColor="#ffff00ff" backgroundColor="#14141464">led2</textLabel>
                </item>
            </IOPad>
            <IOPad id="7" useCaseMode="1">
                <item id="7" caption="PIN 8 (SCL)">
                    <graphics pos="(-308.66,-491.97)" angle="0" flipping="0" hidden="0" tOrigin="(20.00,10.00)"/>
                    <textLabel pos="(6.00,-27.00)" angle="0.00" textColor="#ffff00ff" backgroundColor="#14141464">SCL</textLabel>
                </item>
            </IOPad>
            <IOPad id="8" useCaseMode="1">
                <item id="8" caption="PIN 9 (SDA)">
                    <graphics pos="(-308.66,-438.97)" angle="0" flipping="0" hidden="0" tOrigin="(20.00,10.00)"/>
                    <textLabel pos="(5.50,-27.00)" angle="0.00" textColor="#ffff00ff" backgroundColor="#14141464">SDA</textLabel>
                </item>
            </IOPad>
            <IOPad id="9" useCaseMode="0">
                <item id="9" caption="PIN 10 (IO6)">
                    <graphics pos="(541.84,-496.56)" angle="270" flipping="2" hidden="0" tOrigin="(20.00,10.00)"/>
                </item>
            </IOPad>
            <item id="10" caption="GND (PIN 11)">
                <graphics pos="(629.23,-257.45)" angle="0" flipping="1" hidden="0" tOrigin="(20.00,10.00)"/>
            </item>
            <IOPad id="11" useCaseMode="0">
                <item id="11" caption="PIN 12 (IO7)">
                    <graphics pos="(295.83,-516.19)" angle="0" flipping="1" hidden="0" tOrigin="(20.00,10.00)"/>
                </item>
            </IOPad>
            <IOPad id="12" useCaseMode="0">
                <item id="12" caption="PIN 13 (IO8)">
                    <graphics pos="(162.64,-464.85)" angle="0" flipping="1" hidden="0" tOrigin="(20.00,10.00)"/>
                </item>
            </IOPad>
            <VDDItem id="13">
                <item id="13" caption="VDD2 (PIN 14)">
                    <graphics pos="(626.25,-316.64)" angle="0" flipping="1" hidden="0" tOrigin="(20.00,10.00)"/>
                </item>
            </VDDItem>
            <IOPad id="14" useCaseMode="0">
                <item id="14" caption="PIN 15 (IO9)">
                    <graphics pos="(164.97,-516.79)" angle="0" flipping="1" hidden="0" tOrigin="(20.00,10.00)"/>
                </item>
            </IOPad>
            <IOPad id="15" useCaseMode="0">
                <item id="15" caption="PIN 16 (IO10)">
                    <graphics pos="(303.91,-468.21)" angle="0" flipping="1" hidden="0" tOrigin="(20.00,10.00)"/>
                </item>
            </IOPad>
            <IOPad id="16" useCaseMode="0">
                <item id="16" caption="PIN 17 (IO11)">
                    <graphics pos="(68.98,-473.96)" angle="270" flipping="1" hidden="0" tOrigin="(20.00,10.00)"/>
                </item>
            </IOPad>
            <IOPad id="17" useCaseMode="3">
                <item id="17" caption="PIN 18 (IO12)">
                    <graphics pos="(-128.33,302.01)" angle="180" flipping="3" hidden="0" tOrigin="(20.00,10.00)"/>
                    <textLabel pos="(35.00,47.00)" angle="-180.00" textColor="#ffff00ff" backgroundColor="#14141464">mon</textLabel>
                </item>
            </IOPad>
            <IOPad id="18" useCaseMode="1">
                <item id="18" caption="PIN 19 (IO13)">
                    <graphics pos="(-131.65,-60.37)" angle="180" flipping="3" hidden="0" tOrigin="(20.00,10.00)"/>
                    <textLabel pos="(32.50,47.00)" angle="-180.00" textColor="#ffff00ff" backgroundColor="#14141464">trig</textLabel>
                </item>
            </IOPad>
            <IOPad id="19" useCaseMode="0">
                <item id="19" caption="PIN 20 (IO14)">
                    <graphics pos="(-13.56,-481.59)" angle="270" flipping="1" hidden="0" tOrigin="(20.00,10.00)"/>
                </item>
            </IOPad>
            <item id="20" caption="A CMP0H">
                <graphics pos="(50.00,30.00)" angle="0" flipping="0" hidden="1" tOrigin="(25.00,28.00)"/>
            </item>
            <item id="21" caption="A CMP1H">
                <graphics pos="(150.00,30.00)" angle="0" flipping="0" hidden="1" tOrigin="(25.00,28.00)"/>
            </item>
            <item id="22" caption="A CMP2L">
                <graphics pos="(241.17,294.19)" angle="0" flipping="0" hidden="0" tOrigin="(25.00,28.00)"/>
            </item>
            <item id="23" caption="A CMP3L">
                <graphics pos="(150.00,130.00)" angle="0" flipping="0" hidden="1" tOrigin="(25.00,28.00)"/>
            </item>
            <item id="24" caption="P DLY">
                <graphics pos="(320.00,320.00)" angle="0" flipping="0" hidden="1" tOrigin="(17.50,10.00)"/>
            </item>
            <item id="25" caption="VREF0">
                <graphics pos="(320.00,120.00)" angle="0" flipping="0" hidden="1" tOrigin="(17.50,10.00)"/>
            </item>
            <item id="26" caption="VREF1">
                <graphics pos="(320.00,190.00)" angle="0" flipping="0" hidden="1" tOrigin="(17.50,10.00)"/>
            </item>
            <item id="27" caption="POR">
                <graphics pos="(51.77,-278.65)" angle="270" flipping="0" hidden="0" tOrigin="(17.50,10.00)"/>
            </item>
            <item id="28" caption="OSC0">
                <graphics pos="(-183.99,-309.02)" angle="0" flipping="0" hidden="0" tOrigin="(30.00,40.00)"/>
            </item>
            <item id="29" caption="OSC1">
                <graphics pos="(-70.00,200.00)" angle="0" flipping="0" hidden="1" tOrigin="(30.00,25.00)"/>
            </item>
            <item id="30" caption="OSC2">
                <graphics pos="(-70.00,270.00)" angle="0" flipping="0" hidden="1" tOrigin="(30.00,20.00)"/>
            </item>
            <item id="31" caption="I2C">
                <graphics pos="(-188.66,-510.97)" angle="0" flipping="0" hidden="0" tOrigin="(25.00,45.00)"/>
            </item>
            <item id="32" caption="TEMP SENSOR">
                <graphics pos="(320.00,370.00)" angle="0" flipping="0" hidden="1" tOrigin="(28.00,15.00)"/>
            </item>
            <item id="33" caption="FILTER/EDGE DET">
                <graphics pos="(320.00,440.00)" angle="0" flipping="0" hidden="1" tOrigin="(27.50,15.00)"/>
            </item>
            <item id="34" caption="BG">
                <graphics pos="(320.00,30.00)" angle="0" flipping="0" hidden="1" tOrigin="(17.50,10.00)"/>
            </item>
            <LUT id="35" regularShape="0" mode="0">
                <item id="35" caption="2-bit LUT0/DFF/LATCH0">
                    <graphics pos="(27.40,-63.03)" angle="90" flipping="0" hidden="0" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <LUT id="36" regularShape="0" mode="0">
                <item id="36" caption="2-bit LUT1/DFF/LATCH1">
                    <graphics pos="(622.36,222.96)" angle="90" flipping="0" hidden="0" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <item id="37" caption="2-bit LUT2/DFF/LATCH2">
                <graphics pos="(453.88,221.63)" angle="0" flipping="0" hidden="0" tOrigin="(25.00,10.00)"/>
            </item>
            <LUT id="38" regularShape="0" mode="0">
                <item id="38" caption="2-bit LUT3/PGEN">
                    <graphics pos="(130.00,250.00)" angle="90" flipping="0" hidden="1" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <item id="39" caption="3-bit LUT0/DFF/LATCH3">
                <graphics pos="(163.77,33.14)" angle="0" flipping="2" hidden="0" tOrigin="(25.00,10.00)"/>
            </item>
            <LUT id="40" regularShape="0" mode="0">
                <item id="40" caption="3-bit LUT1/DFF/LATCH4">
                    <graphics pos="(130.00,370.00)" angle="90" flipping="0" hidden="1" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <LUT id="41" regularShape="0" mode="0">
                <item id="41" caption="3-bit LUT2/DFF/LATCH5">
                    <graphics pos="(130.00,430.00)" angle="90" flipping="0" hidden="1" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <LUT id="42" regularShape="0" mode="0">
                <item id="42" caption="3-bit LUT3/DFF/LATCH6">
                    <graphics pos="(210.00,250.00)" angle="90" flipping="0" hidden="1" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <LUT id="43" regularShape="0" mode="0">
                <item id="43" caption="3-bit LUT4/DFF/LATCH7">
                    <graphics pos="(210.00,310.00)" angle="90" flipping="0" hidden="1" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <LUT id="44" regularShape="0" mode="0">
                <item id="44" caption="3-bit LUT5/DFF/LATCH8">
                    <graphics pos="(210.00,370.00)" angle="90" flipping="0" hidden="1" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <LUT id="45" regularShape="0" mode="0">
                <item id="45" caption="3-bit LUT6/Pipe Delay/Ripple Counter">
                    <graphics pos="(210.00,430.00)" angle="90" flipping="0" hidden="1" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <item id="46" caption="MF0 (4-bit LUT0, DFF/LATCH9, WS Ctrl, 16-bit CNT0/DLY0/FSM0)">
                <graphics pos="(-500.00,-20.00)" angle="0" flipping="0" hidden="1" tOrigin="(155.00,60.00)"/>
            </item>
            <item id="47" caption="MF1 (3-bit LUT7, DFF/LATCH10, 8-bit CNT1/DLY1)">
                <graphics pos="(300.97,-82.62)" angle="0" flipping="0" hidden="0" tOrigin="(155.00,60.00)"/>
            </item>
            <item id="48" caption="MF2 (3-bit LUT8, DFF/LATCH11, 8-bit CNT2/DLY2)">
                <graphics pos="(-34.56,302.81)" angle="0" flipping="0" hidden="1" tOrigin="(155.00,60.00)"/>
            </item>
            <item id="49" caption="MF3 (3-bit LUT9, DFF/LATCH12, 8-bit CNT3/DLY3)">
                <graphics pos="(-530.94,-221.98)" angle="0" flipping="0" hidden="1" tOrigin="(155.00,60.00)"/>
            </item>
            <item id="50" caption="MF4 (3-bit LUT10, DFF/LATCH13, 8-bit CNT4/DLY4)">
                <graphics pos="(430.00,-30.00)" angle="0" flipping="0" hidden="1" tOrigin="(155.00,60.00)"/>
            </item>
            <item id="51" caption="MF5 (3-bit LUT11, DFF/LATCH14, 8-bit CNT5/DLY5)">
                <graphics pos="(430.00,130.00)" angle="0" flipping="0" hidden="1" tOrigin="(155.00,60.00)"/>
            </item>
            <item id="52" caption="MF6 (3-bit LUT12, DFF/LATCH15, 8-bit CNT6/DLY6)">
                <graphics pos="(430.00,290.00)" angle="0" flipping="0" hidden="1" tOrigin="(155.00,60.00)"/>
            </item>
            <item id="53" caption="MF7 (3-bit LUT13, DFF/LATCH16, 8-bit CNT7/DLY7)">
                <graphics pos="(430.00,450.00)" angle="0" flipping="0" hidden="1" tOrigin="(155.00,60.00)"/>
            </item>
            <LUT id="54" regularShape="0" mode="0">
                <item id="54" caption="4-bit LUT0 (MF0)">
                    <graphics pos="(-365.00,25.00)" angle="90" flipping="0" hidden="1" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <item id="55" caption="DFF/LATCH9 (MF0)">
                <graphics pos="(-450.00,-20.00)" angle="0" flipping="0" hidden="1" tOrigin="(25.00,10.00)"/>
            </item>
            <CNTDLY id="56" externalClockFrequence="0" externalClockFreqUnit="kHz">
                <item id="56" caption="16-bit CNT0/DLY0/FSM0 (MF0)">
                    <graphics pos="(-450.00,-20.00)" angle="0" flipping="0" hidden="1" tOrigin="(35.00,16.00)"/>
                </item>
            </CNTDLY>
            <LUT id="57" regularShape="0" mode="0">
                <item id="57" caption="3-bit LUT7 (MF1)">
                    <graphics pos="(524.47,-24.12)" angle="90" flipping="0" hidden="0" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <item id="58" caption="DFF/LATCH10 (MF1)">
                <graphics pos="(-450.00,130.00)" angle="0" flipping="0" hidden="1" tOrigin="(25.00,10.00)"/>
            </item>
            <CNTDLY id="59" externalClockFrequence="0" externalClockFreqUnit="kHz">
                <item id="59" caption="8-bit CNT1/DLY1 (MF1)">
                    <graphics pos="(352.47,-38.12)" angle="0" flipping="0" hidden="0" tOrigin="(30.00,16.00)"/>
                </item>
            </CNTDLY>
            <LUT id="60" regularShape="0" mode="0">
                <item id="60" caption="3-bit LUT8 (MF2)">
                    <graphics pos="(100.44,347.81)" angle="90" flipping="0" hidden="1" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <item id="61" caption="DFF/LATCH11 (MF2)">
                <graphics pos="(-550.00,300.00)" angle="0" flipping="0" hidden="1" tOrigin="(25.00,10.00)"/>
            </item>
            <CNTDLY id="62" externalClockFrequence="0" externalClockFreqUnit="kHz">
                <item id="62" caption="8-bit CNT2/DLY2 (MF2)">
                    <graphics pos="(230.80,221.90)" angle="0" flipping="0" hidden="0" tOrigin="(30.00,16.00)"/>
                </item>
            </CNTDLY>
            <LUT id="63" regularShape="0" mode="0">
                <item id="63" caption="3-bit LUT9 (MF3)">
                    <graphics pos="(-395.94,-176.98)" angle="90" flipping="0" hidden="1" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <item id="64" caption="DFF/LATCH12 (MF3)">
                <graphics pos="(-730.00,460.00)" angle="0" flipping="0" hidden="1" tOrigin="(25.00,10.00)"/>
            </item>
            <CNTDLY id="65" externalClockFrequence="0" externalClockFreqUnit="kHz">
                <item id="65" caption="8-bit CNT3/DLY3 (MF3)">
                    <graphics pos="(46.79,-193.76)" angle="0" flipping="0" hidden="0" tOrigin="(30.00,16.00)"/>
                </item>
            </CNTDLY>
            <LUT id="66" regularShape="0" mode="0">
                <item id="66" caption="3-bit LUT10 (MF4)">
                    <graphics pos="(565.00,15.00)" angle="90" flipping="0" hidden="1" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <item id="67" caption="DFF/LATCH13 (MF4)">
                <graphics pos="(660.00,-210.00)" angle="0" flipping="0" hidden="1" tOrigin="(25.00,10.00)"/>
            </item>
            <CNTDLY id="68" externalClockFrequence="0" externalClockFreqUnit="kHz">
                <item id="68" caption="8-bit CNT4/DLY4 (MF4)">
                    <graphics pos="(660.00,-210.00)" angle="0" flipping="0" hidden="1" tOrigin="(30.00,16.00)"/>
                </item>
            </CNTDLY>
            <LUT id="69" regularShape="0" mode="0">
                <item id="69" caption="3-bit LUT11 (MF5)">
                    <graphics pos="(565.00,175.00)" angle="90" flipping="0" hidden="1" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <item id="70" caption="DFF/LATCH14 (MF5)">
                <graphics pos="(500.00,-50.00)" angle="0" flipping="0" hidden="1" tOrigin="(25.00,10.00)"/>
            </item>
            <CNTDLY id="71" externalClockFrequence="0" externalClockFreqUnit="kHz">
                <item id="71" caption="8-bit CNT5/DLY5 (MF5)">
                    <graphics pos="(500.00,-50.00)" angle="0" flipping="0" hidden="1" tOrigin="(30.00,16.00)"/>
                </item>
            </CNTDLY>
            <LUT id="72" regularShape="0" mode="0">
                <item id="72" caption="3-bit LUT12 (MF6)">
                    <graphics pos="(565.00,335.00)" angle="90" flipping="0" hidden="1" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <item id="73" caption="DFF/LATCH15 (MF6)">
                <graphics pos="(330.00,110.00)" angle="0" flipping="0" hidden="1" tOrigin="(25.00,10.00)"/>
            </item>
            <CNTDLY id="74" externalClockFrequence="0" externalClockFreqUnit="kHz">
                <item id="74" caption="8-bit CNT6/DLY6 (MF6)">
                    <graphics pos="(330.00,110.00)" angle="0" flipping="0" hidden="1" tOrigin="(30.00,16.00)"/>
                </item>
            </CNTDLY>
            <LUT id="75" regularShape="0" mode="0">
                <item id="75" caption="3-bit LUT13 (MF7)">
                    <graphics pos="(565.00,495.00)" angle="90" flipping="0" hidden="1" tOrigin="(20.00,15.00)"/>
                </item>
            </LUT>
            <item id="76" caption="DFF/LATCH16 (MF7)">
                <graphics pos="(170.00,270.00)" angle="0" flipping="0" hidden="1" tOrigin="(25.00,10.00)"/>
            </item>
            <CNTDLY id="77" externalClockFrequence="0" externalClockFreqUnit="kHz">
                <item id="77" caption="8-bit CNT7/DLY7 (MF7)">
                    <graphics pos="(170.00,270.00)" angle="0" flipping="0" hidden="1" tOrigin="(30.00,16.00)"/>
                </item>
            </CNTDLY>
            <EEPROM id="78">
                <data>0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0</data>
                <item id="78" caption="EEPROM">
                    <graphics pos="(-70.00,48.00)" angle="0" flipping="0" hidden="1" tOrigin="(30.00,16.00)"/>
                </item>
            </EEPROM>
            <wire output="147" input="111" autoRouting="1" pen="#ff8000ff;1.00;1;32;128" lineType="2" protected="1" CWLid="0" wireText="NET0" wireState="0">
                <points>(-247.00,-481.00); (-210.00,-481.00)</points>
            </wire>
            <wire output="148" input="112" autoRouting="1" pen="#ff8000ff;1.00;1;32;128" lineType="2" protected="1" CWLid="1" wireText="NET1" wireState="0">
                <points>(-247.00,-428.00); (-220.00,-428.00); (-220.00,-451.00); (-210.00,-451.00)</points>
            </wire>
            <wire output="194" input="659" autoRouting="1" pen="#ff8000ff;1.00;1;32;128" lineType="2" protected="1" CWLid="7" wireText="NET7" wireState="0">
                <points>(432.00,-23.00); (508.00,-23.00)</points>
            </wire>
            <wire output="143" input="625" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="9" wireText="NET9" wireState="0">
                <points>(-68.00,121.00); (496.00,121.00); (496.00,4.00); (508.00,4.00)</points>
            </wire>
            <wire output="161" input="549" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="10" wireText="NET10" wireState="0">
                <points>(234.00,43.00); (240.00,43.00); (240.00,65.00); (124.00,65.00); (124.00,39.00); (143.00,39.00)</points>
            </wire>
            <wire output="161" input="626" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="10" wireText="NET10" wireState="0">
                <points>(234.00,43.00); (502.00,43.00); (502.00,-9.00); (508.00,-9.00)</points>
            </wire>
            <wire output="39" input="550" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="-1" wireText="POR" wireState="1">
                <points/>
            </wire>
            <wire output="156" input="262" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="11" wireText="NET11" wireState="0">
                <points>(-70.00,-56.00); (8.00,-56.00)</points>
            </wire>
            <wire output="84" input="548" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="12" wireText="NET12" wireState="0">
                <points>(86.00,-48.00); (99.41,-48.00); (99.41,49.00); (143.00,49.00)</points>
            </wire>
            <wire output="43" input="634" autoRouting="1" pen="#ff8000ff;1.00;1;32;128" lineType="2" protected="1" CWLid="-1" wireText="OSC0 CLK /64" wireState="1">
                <points/>
            </wire>
            <wire output="39" input="635" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="-1" wireText="POR" wireState="1">
                <points/>
            </wire>
            <wire output="198" input="261" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="13" wireText="READY" wireState="1">
                <points/>
            </wire>
            <wire output="159" input="543" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="15" wireText="NET15" wireState="0">
                <points>(524.00,231.00); (597.00,231.00); (597.00,230.00); (603.00,230.00)</points>
            </wire>
            <wire output="159" input="545" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="15" wireText="NET15" wireState="0">
                <points>(524.00,231.00); (530.00,231.00); (530.00,257.00); (412.00,257.00); (412.00,227.00); (433.00,227.00)</points>
            </wire>
            <wire output="42" input="630" autoRouting="1" pen="#ff8000ff;1.00;1;32;128" lineType="2" protected="1" CWLid="-1" wireText="OSC0 CLK /8" wireState="1">
                <points/>
            </wire>
            <wire output="39" input="631" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="-1" wireText="POR" wireState="1">
                <points/>
            </wire>
            <wire output="196" input="544" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="16" wireText="NET16" wireState="0">
                <points>(311.00,237.00); (433.00,237.00)</points>
            </wire>
            <wire output="33" input="542" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="17" wireText="NET17" wireState="0">
                <points>(311.00,322.00); (580.00,322.00); (580.00,246.00); (603.00,246.00)</points>
            </wire>
            <wire output="39" input="94" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="-1" wireText="POR" wireState="1">
                <points/>
            </wire>
            <wire output="155" input="92" autoRouting="1" pen="#ff8000ff;1.00;1;32;128" lineType="2" protected="1" CWLid="18" wireText="NET18" wireState="0">
                <points>(-66.00,307.00); (220.00,307.00)</points>
            </wire>
            <wire output="42" input="682" autoRouting="1" pen="#ff8000ff;1.00;1;32;128" lineType="2" protected="1" CWLid="-1" wireText="OSC0 CLK /8" wireState="1">
                <points/>
            </wire>
            <wire output="0" input="105" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="-1" wireText="VDD" wireState="1">
                <points/>
            </wire>
            <wire output="84" input="627" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="12" wireText="NET12" wireState="0">
                <points>(86.00,-48.00); (325.00,-48.00); (325.00,-18.00); (331.00,-18.00)</points>
            </wire>
            <wire output="0" input="509" autoRouting="1" pen="#ff8000ff;1.00;1;32;128" lineType="2" protected="1" CWLid="-1" wireText="VDD" wireState="1">
                <points/>
            </wire>
            <wire output="158" input="508" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="14" wireText="NET14" wireState="0">
                <points>(681.00,238.00); (759.00,238.00)</points>
            </wire>
            <wire output="0" input="497" autoRouting="1" pen="#ff8000ff;1.00;1;32;128" lineType="2" protected="1" CWLid="-1" wireText="VDD" wireState="1">
                <points/>
            </wire>
            <wire output="193" input="496" autoRouting="1" pen="#00ff00ff;1.00;1;32;128" lineType="1" protected="0" CWLid="8" wireText="NET8" wireState="0">
                <points>(579.00,-9.00); (763.00,-9.00)</points>
            </wire>
        </chip>
        <emulatorConfiguration version="4" oldestCompatibleVersion="4">
            <settings>
                <autoApply value="0"/>
                <programmingOptions programNVM="1" programEEPROM="0"/>
                <platformSelector id="1"/>
            </settings>
            <platform id="0" friendlyName="GreenPAK DIP Development Platform">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="1" friendlyName="GreenPAK Advanced Development Platform">
                <lastConfiguration modified="1">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector>1:0;2:0;3:0;4:0;5:0;6:0;7:0;8:0;9:0;10:0;11:0;12:0;13:0;14:0;15:0;16:0;17:0;18:0;19:0;20:0</ExpansionConnector>
                        <TestPoints>
                            <TPC ID="1" Type="8">
                                <BaseOption LEDEnable="0" LEDInvertion="0" HotKey="81" GlobalLink="0"/>
                                <GeneratorOpt GenType="5">
                                    <constantVoltageGenerator v="2.999927e+00|4">
                                        <abstractGenerator repeat="0" repeatCount="0" shownPeriod="0" startPoint="0.000000e+00|5" stopPoint="6.000000e+03|5" pauseState="0" prestartState="1" outputState="0" prestartDelay="0.000000e+00|5" endState="0" link="0" sync="0"/>
                                    </constantVoltageGenerator>
                                </GeneratorOpt>
                            </TPC>
                            <TPC ID="2" Type="1">
                                <BaseOption LEDEnable="0" LEDInvertion="0" HotKey="87" GlobalLink="1"/>
                            </TPC>
                            <TPC ID="3" Type="1">
                                <BaseOption LEDEnable="1" LEDInvertion="0" HotKey="69" GlobalLink="1"/>
                            </TPC>
                            <TPC ID="4" Type="6">
                                <BaseOption LEDEnable="1" LEDInvertion="0" HotKey="82" GlobalLink="1"/>
                                <ButtonSettings UpSide="1" DownSide="0" LatchMode="1" DefaultConnection="1" ConnectedSide="1"/>
                            </TPC>
                            <TPC ID="5" Type="6">
                                <BaseOption LEDEnable="1" LEDInvertion="0" HotKey="84" GlobalLink="1"/>
                                <ButtonSettings UpSide="1" DownSide="0" LatchMode="0" DefaultConnection="1" ConnectedSide="1"/>
                            </TPC>
                            <TPC ID="6" Type="1">
                                <BaseOption LEDEnable="1" LEDInvertion="0" HotKey="89" GlobalLink="1"/>
                            </TPC>
                            <TPC ID="7" Type="1">
                                <BaseOption LEDEnable="1" LEDInvertion="0" HotKey="85" GlobalLink="1"/>
                            </TPC>
                            <TPC ID="8" Type="4">
                                <BaseOption LEDEnable="0" LEDInvertion="0" HotKey="73" GlobalLink="1"/>
                            </TPC>
                            <TPC ID="9" Type="4">
                                <BaseOption LEDEnable="0" LEDInvertion="0" HotKey="79" GlobalLink="1"/>
                            </TPC>
                            <TPC ID="10" Type="1">
                                <BaseOption LEDEnable="1" LEDInvertion="0" HotKey="80" GlobalLink="1"/>
                            </TPC>
                            <TPC ID="11" Type="3">
                                <BaseOption LEDEnable="0" LEDInvertion="0" HotKey="-1" GlobalLink="1"/>
                            </TPC>
                            <TPC ID="12" Type="1">
                                <BaseOption LEDEnable="0" LEDInvertion="0" HotKey="70" GlobalLink="1"/>
                            </TPC>
                            <TPC ID="13" Type="1">
                                <BaseOption LEDEnable="0" LEDInvertion="0" HotKey="83" GlobalLink="1"/>
                            </TPC>
                            <TPC ID="14" Type="8">
                                <BaseOption LEDEnable="0" LEDInvertion="0" HotKey="68" GlobalLink="0"/>
                                <GeneratorOpt GenType="5">
                                    <constantVoltageGenerator v="2.999927e+00|4">
                                        <abstractGenerator repeat="0" repeatCount="0" shownPeriod="0" startPoint="0.000000e+00|5" stopPoint="6.000000e+03|5" pauseState="0" prestartState="1" outputState="0" prestartDelay="0.000000e+00|5" endState="0" link="0" sync="0"/>
                                    </constantVoltageGenerator>
                                </GeneratorOpt>
                            </TPC>
                            <TPC ID="15" Type="1">
                                <BaseOption LEDEnable="0" LEDInvertion="0" HotKey="65" GlobalLink="1"/>
                            </TPC>
                            <TPC ID="16" Type="1">
                                <BaseOption LEDEnable="0" LEDInvertion="0" HotKey="71" GlobalLink="1"/>
                            </TPC>
                            <TPC ID="17" Type="1">
                                <BaseOption LEDEnable="0" LEDInvertion="0" HotKey="74" GlobalLink="1"/>
                            </TPC>
                            <TPC ID="18" Type="8">
                                <BaseOption LEDEnable="0" LEDInvertion="0" HotKey="75" GlobalLink="1"/>
                                <GeneratorOpt GenType="6">
                                    <sineGenerator phase="1" phaseValue="0.000" amplitude="1.400000e+00|4" offset="1.500000e+00|4"/>
                                    <userDefinedGenerator>
                                        <data>(0,1107); (1001,1215); (2002,1321); (3003,1426); (4004,1527); (5005,1623); (6006,1714); (7007,1798); (8008,1875); (9009,1943); (10010,2002); (11011,2051); (12012,2089); (13013,2117); (14014,2134); (15015,2139); (16016,2134); (17017,2117); (18018,2088); (19019,2049); (20020,2000); (21021,1941); (22022,1873); (23023,1796); (24024,1712); (25025,1621); (26026,1524); (27027,1423); (28028,1318); (29029,1211); (30030,1103); (31031,995); (32032,888); (33033,784); (34034,683); (35035,587); (36036,496); (37037,412); (38038,336); (39039,268); (40040,210); (41041,161); (42042,123); (43043,95); (44044,79); (45045,74); (46046,80); (47047,97); (48048,126); (49049,165); (50050,215); (51051,274); (52052,343); (53053,420); (54054,504); (55055,595); (56056,692); (57057,793); (58058,898); (59059,1005); (60000,1107)</data>
                                        <visibleFlags>1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1; 1</visibleFlags>
                                        <abstractGenerator repeat="0" repeatCount="2" shownPeriod="0" startPoint="0.000000e+00|5" stopPoint="6.000000e+03|5" pauseState="0" prestartState="0" outputState="0" prestartDelay="0.000000e+00|5" endState="0" link="1" sync="0"/>
                                    </userDefinedGenerator>
                                </GeneratorOpt>
                            </TPC>
                            <TPC ID="19" Type="6">
                                <BaseOption LEDEnable="0" LEDInvertion="0" HotKey="76" GlobalLink="1"/>
                                <ButtonSettings UpSide="3" DownSide="0" LatchMode="0" DefaultConnection="1" ConnectedSide="1"/>
                            </TPC>
                            <TPC ID="20" Type="1">
                                <BaseOption LEDEnable="0" LEDInvertion="0" HotKey="92" GlobalLink="1"/>
                            </TPC>
                        </TestPoints>
                        <I2C slaveAddress="-1"/>
                        <TestPointsOrder>1;14;18</TestPointsOrder>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="2" friendlyName="GreenPAK Pro Development Platform">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="4" friendlyName="GreenPAK Serial Debugger">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="5" friendlyName="GreenPAK Advanced Development Platform w/ Logic Level Adapter #1">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="6" friendlyName="ForgeFPGA Advanced Development Platform">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="7" friendlyName="ForgeFPGA Evaluation Board">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="8" friendlyName="SLG51000 Demo Board">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="9" friendlyName="SLG51001 Demo Board">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="10" friendlyName="SLG51002 Demo Board">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="11" friendlyName="GreenPAK Serial Debugger">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="12" friendlyName="GreenPAK Lite Development Platform">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="13" friendlyName="HVPAK Demo Board">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="14" friendlyName="SLG47105V Training Board">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="15" friendlyName="PowerPAK Development Platform">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
            <platform id="16" friendlyName="ForgeFPGA Advanced Development Platform Rev. 2.0">
                <lastConfiguration modified="0">
                    <SaveEmulator Name="Default">
                        <PowerOptions synced="0"/>
                        <ExternalChipConnectionSource source="0"/>
                        <PowerSwitch internalPower="1" externalPower="0"/>
                        <ExpansionConnector></ExpansionConnector>
                        <TestPoints/>
                        <I2C slaveAddress="-1"/>
                    </SaveEmulator>
                </lastConfiguration>
                <savedConfigurations/>
            </platform>
        </emulatorConfiguration>
        <simulationConfiguration version="16" compatibleVersion="16" activePreset="-1">
            <draftPreset>
                <simulationPreset index="-1" name="Default" customGroupLayout="true" customParametricDcGroupLayout="false">
                    <transientAnalyses>
                        <transientAnalysis stopTime="2" maxTimeStep="20u" startTime="0" stepTime="20u" temperature="25" useInitialConditions="false" vdd="3.3"/>
                    </transientAnalyses>
                    <parametricDcAnalyses/>
                    <pinProbes>
                        <pinProbe instrumentId="0" measurementFlags="1">
                            <IdDto category="5" componentType="43" componentNumber="1" pinNumber="0"/>
                        </pinProbe>
                        <pinProbe instrumentId="1" measurementFlags="1">
                            <IdDto category="5" componentType="43" componentNumber="2" pinNumber="0"/>
                        </pinProbe>
                        <pinProbe instrumentId="4" measurementFlags="1">
                            <IdDto category="100" componentType="45" componentNumber="0" pinNumber="12"/>
                        </pinProbe>
                        <pinProbe instrumentId="5" measurementFlags="1">
                            <IdDto category="100" componentType="45" componentNumber="0" pinNumber="16"/>
                        </pinProbe>
                    </pinProbes>
                    <groups>
                        <group name="V1 -&gt; n+" customGroupLayout="false">
                            <waveforms>
                                <WaveformIdData analysisType="0" pinIdStr="5;43;1;0" xAxisBinding="0;;-1;-1;-1">
                                    <parameters/>
                                </WaveformIdData>
                            </waveforms>
                        </group>
                        <group name="V2 -&gt; n+ [ext_vdd]" customGroupLayout="false">
                            <waveforms>
                                <WaveformIdData analysisType="0" pinIdStr="5;43;2;0" xAxisBinding="0;;-1;-1;-1">
                                    <parameters/>
                                </WaveformIdData>
                            </waveforms>
                        </group>
                        <group name="GreenPAK -&gt; PIN 16 &lt;- EXT. IN/OUT" customGroupLayout="true">
                            <waveforms>
                                <WaveformIdData analysisType="0" pinIdStr="100;45;0;16" xAxisBinding="0;;-1;-1;-1">
                                    <parameters/>
                                </WaveformIdData>
                            </waveforms>
                        </group>
                        <group name="GreenPAK -&gt; PIN 12 &lt;- EXT. OUT" customGroupLayout="false">
                            <waveforms>
                                <WaveformIdData analysisType="0" pinIdStr="100;45;0;12" xAxisBinding="0;;-1;-1;-1">
                                    <parameters/>
                                </WaveformIdData>
                            </waveforms>
                        </group>
                    </groups>
                    <parametricDcGroups/>
                    <waveforms>
                        <waveform>
                            <waveformSetup penColor="#26e056" penWidth="2" style="0" attributes="1" symbol="-1" symSize="6" symColor="#ff0000"/>
                            <WaveformIdData analysisType="0" pinIdStr="5;43;1;0" xAxisBinding="0;;-1;-1;-1">
                                <parameters/>
                            </WaveformIdData>
                        </waveform>
                        <waveform>
                            <waveformSetup penColor="#2e8eff" penWidth="2" style="0" attributes="1" symbol="-1" symSize="6" symColor="#ff0000"/>
                            <WaveformIdData analysisType="0" pinIdStr="5;43;2;0" xAxisBinding="0;;-1;-1;-1">
                                <parameters/>
                            </WaveformIdData>
                        </waveform>
                        <waveform>
                            <waveformSetup penColor="#fda740" penWidth="2" style="0" attributes="1" symbol="-1" symSize="6" symColor="#ff0000"/>
                            <WaveformIdData analysisType="0" pinIdStr="100;45;0;12" xAxisBinding="0;;-1;-1;-1">
                                <parameters/>
                            </WaveformIdData>
                        </waveform>
                        <waveform>
                            <waveformSetup penColor="#46f8ff" penWidth="2" style="0" attributes="1" symbol="-1" symSize="6" symColor="#ff0000"/>
                            <WaveformIdData analysisType="0" pinIdStr="100;45;0;16" xAxisBinding="0;;-1;-1;-1">
                                <parameters/>
                            </WaveformIdData>
                        </waveform>
                    </waveforms>
                    <components>
                        <component simulationModel="" defaultSimulationModel="">
                            <componentId category="5" componentType="0" componentNumber="1"/>
                            <componentUiSettings isFlippedHorizontally="false" isFlippedVertically="false" visible="true" position="(255.984;-252.445)" rotationState="0" sceneIndex="0"/>
                            <schematicProps>
                                <param id="name" affinity="4" value="GND" defaultValue=""/>
                                <param id="mfg" affinity="4" value="" defaultValue=""/>
                                <param id="part_number" affinity="4" value="" defaultValue=""/>
                            </schematicProps>
                            <instanceProps/>
                        </component>
                        <component simulationModel="" defaultSimulationModel="">
                            <componentId category="5" componentType="0" componentNumber="2"/>
                            <componentUiSettings isFlippedHorizontally="false" isFlippedVertically="false" visible="true" position="(862.016;-253.143)" rotationState="0" sceneIndex="0"/>
                            <schematicProps>
                                <param id="name" affinity="4" value="GND" defaultValue=""/>
                                <param id="mfg" affinity="4" value="" defaultValue=""/>
                                <param id="part_number" affinity="4" value="" defaultValue=""/>
                            </schematicProps>
                            <instanceProps/>
                        </component>
                        <component simulationModel="" defaultSimulationModel="">
                            <componentId category="5" componentType="0" componentNumber="3"/>
                            <componentUiSettings isFlippedHorizontally="false" isFlippedVertically="false" visible="true" position="(707.317;-193.802)" rotationState="0" sceneIndex="0"/>
                            <schematicProps>
                                <param id="name" affinity="4" value="GND" defaultValue=""/>
                                <param id="mfg" affinity="4" value="" defaultValue=""/>
                                <param id="part_number" affinity="4" value="" defaultValue=""/>
                            </schematicProps>
                            <instanceProps/>
                        </component>
                        <component simulationModel="" defaultSimulationModel="">
                            <componentId category="5" componentType="43" componentNumber="1"/>
                            <componentUiSettings isFlippedHorizontally="false" isFlippedVertically="false" visible="true" position="(324.756;-325.994)" rotationState="0" sceneIndex="0"/>
                            <schematicProps>
                                <param id="name" affinity="4" value="V1" defaultValue=""/>
                                <param id="mfg" affinity="4" value="" defaultValue=""/>
                                <param id="part_number" affinity="4" value="" defaultValue=""/>
                                <param id="has_rc" affinity="1" value="1" defaultValue=""/>
                                <param id="int_r" affinity="3" value="10" defaultValue=""/>
                                <param id="int_c" affinity="3" value="100n" defaultValue=""/>
                                <param id="show_one_period" affinity="1" value="0" defaultValue=""/>
                                <param id="has_limited_voltage" affinity="1" value="0" defaultValue=""/>
                                <param id="dc_analysis_voltage" affinity="3" value="3.3" defaultValue=""/>
                                <param id="signal_type" affinity="1" value="1" defaultValue=""/>
                                <param id="prestart_delay" affinity="3" value="0" defaultValue=""/>
                                <param id="prestart_state" affinity="1" value="0" defaultValue=""/>
                                <param id="repeat_state" affinity="1" value="0" defaultValue=""/>
                                <param id="repeat_count" affinity="1" value="2" defaultValue=""/>
                                <param id="end_state" affinity="1" value="1" defaultValue=""/>
                                <param id="ramp_voltage" affinity="3" value="3.3" defaultValue=""/>
                                <param id="ramp_rise_time" affinity="3" value="1m" defaultValue=""/>
                            </schematicProps>
                            <instanceProps/>
                        </component>
                        <component simulationModel="" defaultSimulationModel="">
                            <componentId category="5" componentType="43" componentNumber="2"/>
                            <componentUiSettings isFlippedHorizontally="true" isFlippedVertically="false" visible="true" position="(783.242;-326.965)" rotationState="0" sceneIndex="0"/>
                            <schematicProps>
                                <param id="name" affinity="4" value="V2" defaultValue=""/>
                                <param id="mfg" affinity="4" value="" defaultValue=""/>
                                <param id="part_number" affinity="4" value="" defaultValue=""/>
                                <param id="has_rc" affinity="1" value="1" defaultValue=""/>
                                <param id="int_r" affinity="3" value="10" defaultValue=""/>
                                <param id="int_c" affinity="3" value="100n" defaultValue=""/>
                                <param id="show_one_period" affinity="1" value="0" defaultValue=""/>
                                <param id="has_limited_voltage" affinity="1" value="1" defaultValue=""/>
                                <param id="dc_analysis_voltage" affinity="3" value="3.3" defaultValue=""/>
                                <param id="signal_type" affinity="1" value="1" defaultValue=""/>
                                <param id="prestart_delay" affinity="3" value="0" defaultValue=""/>
                                <param id="prestart_state" affinity="1" value="0" defaultValue=""/>
                                <param id="repeat_state" affinity="1" value="0" defaultValue=""/>
                                <param id="repeat_count" affinity="1" value="2" defaultValue=""/>
                                <param id="end_state" affinity="1" value="1" defaultValue=""/>
                                <param id="ramp_voltage" affinity="3" value="3.3" defaultValue=""/>
                                <param id="ramp_rise_time" affinity="3" value="1m" defaultValue=""/>
                            </schematicProps>
                            <instanceProps/>
                        </component>
                    </components>
                    <networks>
                        <network networkId="6" name="NET6">
                            <connections>
                                <connection connectionType="0" routingType="0" sceneIndex="0">
                                    <from>
                                        <IdDto category="5" componentType="43" componentNumber="1" pinNumber="1"/>
                                    </from>
                                    <to>
                                        <IdDto category="5" componentType="0" componentNumber="1" pinNumber="0"/>
                                    </to>
                                    <path>
                                        <point value="(303;-305)"/>
                                        <point value="(272;-305)"/>
                                        <point value="(272;-274)"/>
                                    </path>
                                </connection>
                            </connections>
                        </network>
                        <network networkId="5" name="NET5">
                            <connections>
                                <connection connectionType="0" routingType="0" sceneIndex="0">
                                    <from>
                                        <IdDto category="5" componentType="43" componentNumber="1" pinNumber="0"/>
                                    </from>
                                    <to>
                                        <IdDto category="100" componentType="45" componentNumber="0" pinNumber="1"/>
                                    </to>
                                    <path>
                                        <point value="(388;-305)"/>
                                        <point value="(461;-305)"/>
                                    </path>
                                </connection>
                            </connections>
                        </network>
                        <network networkId="4" name="ext_vdd">
                            <connections>
                                <connection connectionType="0" routingType="0" sceneIndex="0">
                                    <from>
                                        <IdDto category="5" componentType="43" componentNumber="2" pinNumber="0"/>
                                    </from>
                                    <to>
                                        <IdDto category="100" componentType="45" componentNumber="0" pinNumber="14"/>
                                    </to>
                                    <path>
                                        <point value="(761;-306)"/>
                                        <point value="(688;-306)"/>
                                    </path>
                                </connection>
                            </connections>
                        </network>
                        <network networkId="3" name="NET3">
                            <connections>
                                <connection connectionType="0" routingType="0" sceneIndex="0">
                                    <from>
                                        <IdDto category="5" componentType="0" componentNumber="2" pinNumber="0"/>
                                    </from>
                                    <to>
                                        <IdDto category="5" componentType="43" componentNumber="2" pinNumber="1"/>
                                    </to>
                                    <path>
                                        <point value="(878;-275)"/>
                                        <point value="(878;-306)"/>
                                        <point value="(846;-306)"/>
                                    </path>
                                </connection>
                            </connections>
                        </network>
                        <network networkId="2" name="ext-gnd">
                            <connections>
                                <connection connectionType="0" routingType="0" sceneIndex="0">
                                    <from>
                                        <IdDto category="5" componentType="0" componentNumber="3" pinNumber="0"/>
                                    </from>
                                    <to>
                                        <IdDto category="100" componentType="45" componentNumber="0" pinNumber="11"/>
                                    </to>
                                    <path>
                                        <point value="(723;-216)"/>
                                        <point value="(723;-247)"/>
                                        <point value="(691;-247)"/>
                                    </path>
                                </connection>
                            </connections>
                        </network>
                    </networks>
                </simulationPreset>
            </draftPreset>
            <simulationPresets/>
        </simulationConfiguration>
        <projectData>
            <specs>
                <lastModify lastModifyValue="30.08.2024 15:57:37"/>
                <vddSpecs vddMin="2.8" vddTyp="3" vddMax="3.3"/>
                <vdd2Specs vdd2Min="2.8" vdd2Typ="3" vdd2Max="3.3"/>
                <tempSpecs tempMin="-5" tempTyp="20" tempMax="35"/>
            </specs>
            <projectDataFields>
                <textLineDataField name="Customer Name" id="2" text=""/>
                <textLineDataField name="Customer Project Name" id="3" text=""/>
                <textLineDataField name="Customer Project Number" id="4" text=""/>
                <textLineDataField name="Customer Version Number" id="5" text=""/>
                <multiTextLineDataField>
                    <textLineDataField name="Notes" id="6" text=""/>
                </multiTextLineDataField>
            </projectDataFields>
        </projectData>
        <i2cTool>
            <i2cDebugger version="1"/>
            <i2cStepper version="1" rowCount="0"/>
            <i2cRegsTable version="1" tabCount="0"/>
        </i2cTool>
    <logicAnalyzer>
        <metadata>
            <autosavePreset>-1</autosavePreset>
            <currentPreset>-1</currentPreset>
            <version>3</version>
        </metadata>
        <presetList/>
    </logicAnalyzer>
    
    </GPDProject>
    

    On my system I see the lock-up doing this:

     

    Select emulation on the ADB.

    LED on pin 7 is flashing.

     

    Set button on pin 4 to GND.

    Click button on pin 19. Observe LED on pin 3 toggles on/off with each press.

     

    Set button on pin 4 to VCC

    Click button on pin 19. Observe LED on pin 3 flash on for brief period with each press.

     

    Start generator on pin 4.

    Observe LED on pin 7 is on, then flashes; repeats over 6 seconds.

     

    Repeat sequence of setting buttons on pins 4 and 19 – after a few trials the board stops responding.

    The design is still operating, but has lost communication with the GUI.

    Recovery only by disconnecting the USB lead.

     

  • I have raised a support ticket, since the design has to be finished imminently and the board fault can worked around, but slows testing considerably.

  • Humm...
    I was not able to confirm this issue using ADB.
    Shouldn't you suspect an ADB glitch?
    Over