Hi,
For one of our customers, Im am trying to implement a PWM Frequency Converter from 400Hz fixed frequency to 2KHz fixed frequency using SLG46826V. However, I couldn't make it.
I have checked the PWM Frequency Conversion example, there is a PWM Block which SLG46826V doesn't have. I have checked other PWM examples. The concept is okay but, I couldn't get the DUTY adjusted. Ideally, I want to read the duty from the 400Hz PWM signal and write it to 2KHz PWM signal. How can I achieve this application using SLG46826V? I have a board with SLG46826V, and we have some in stock. Also the quantity is low, therefore the customer will program them during production. Regards,
Caner Alp Electronix
For this task you need GreenPak with DCMP like SLG46140/ SLG46620
Thanks
AB
Please see the conversation above.
This AN-CM-271 application note (.GP) file is developed on SLG46140 , Kindly use the same chip for understanding/working.
You are using SLG46621 and for each block you need check their properties also.
Also check the link .GP file for AN_CM_271