This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

PLC CPX4 and Audio

Has anybody used the CPX4 for voice audio? We are looking at using the CPX4 in a fire panel phone system with up to 20 phones on a 1km loop.

We purchased  2 Renesas CPX4 DC kits for testing with various cable types, and seems to operate over 2km of fire rated cable in CPX mode with out any problems.

We purchased 2 Renesas CPX3 + Audio kits to test Audio over PLC and seems to work well.

There doesn't seem to be any demo software available from Renesas for sending audio with the CPX4.  

We are attempting to get the SDK from Renesas for the CPX3 and CPX4 so we can write our own code to run on  the RX651 MPU on the kits, and also the source code for the audio demo software (if available) so we can modify it. So far we have hand no responses from Renesas Singapore. Does anybody have any suggestions on who to contact at Renesas regarding software support for PLC?

Regards,

Hugh

Johnson Controls Ltd NZ.  




[locked by: Cindy H at 12:15 (GMT 0) on 30 Nov 2023]
Parents
  • Thanks for submitting this same inquiry through our website's our technical support system. That is the best way to get support on this product. One of the online apps engineers who is responsible for this product will be responding to you through the technical support system today or tomorrow.

    Best regards, Cindy

  • Hi Cindy, we are yet to hear back from one of the apps engineers. Regards, Hugh

  • Hi Hugh,

    I see that the apps engineer has replied to your Ticket #379432.

    Best regards,

    Cindy

  • Hi Cindy,

    I got the message below from Kazuaki Chikuki, but have yet to hear from a "member of the team from our area". Note if this is Kah Wei Lim <[email protected]> or Leon Sae-Ung <[email protected]> we haven't heard from them since about 13th Nov.

    Regards,

    Hugh 

    Support Ticket Updated
    The following support ticket was updated. After you sign into the Customer Hub https://en-support.renesas.com, you can view the ticket in "TICKET" menu. You can also add questions with the "New Comment" button.
    Please use "SUBMIT A TICKET" for a new question.

    Hi Cindy,

    Ticket Number: 379432
    Date Created: 11/27/2023 3:12 PM
    Topic: CPX4 PLC Modem - Software Support

    If you would like to add additional information to this ticket, simply reply to this email. To ensure proper delivery, include the ticket number in brackets in the subject line.
    Response
    Hello Hugh,

    I have sent your request to our team who covers your area and a member of their team should be contacting you directly. I will close out this ticket, but if you don’t hear from anyone in a timely manner you may reopen this ticket at any time by replying to this email.

    Best Regards,
    Kazuaki Chikuki
    ________________________________________
    11/28/2023 2:15 AM
    Description
    Who do we contact at Renesas to obtain the SDK for the CPX3 and CPX4 PLC chips so we can write our own code to run on the RX651 MPU on the Renesas CPX3 and CPX4 kits?

    Can the CPX4 be used for Voice over PLC applications, as per the CPX3?

    Is the source code for the Renesas Voice over PLC Sample Application and or the Renesas PLC Voice Communicator application available?

    Are the schematics and PCB layouts shown in the R30AN0393EJ0100 CPX4 DC-PLC Evaluation Kit M01D1 – RTK0EE0009D01001BJ SCH, BOM, PCB Layout document available as Altium Designer or other electronic format?

    Note we have been attempting to obtain the above information from Renesas Singapore for several weeks.

    Regards,

    Hugh

    ________________________________________
    11/27/2023 3:12 PM


    < check out our Renesas community support for popular products on Renesas Community >

  • Hello Hugh,

    Please log in to your account and find the Ticket and update that ticket with this information. This way Chikuki-san will know these additional details. 

    Best regards, Cindy

Reply Children
No Data