ISL3259E transition from transmit to receive operation

Hi,

I'm using the ISL3259E RS485 transceiver and I'm getting a bit error when changing from transmit enable to receive enable. Following the change on the RE/DE pin a bit the RO line goes from high to low (start bit condition). The RS485 line is terminated but not being driven by another devices (also tried with another device on the bus). The RE/DE pins are tied together so are transitioning at the same time.

The attached images shows the issue. The bus is terminated but not driven by any other devices.

The traces are connected to the following nets:

pink: DE/RE

blue: RS485 bus (differential probe A-B)

yellow: RO

It looks to me that The transceiver is briefly in transmit and receive at the same time.

Any insight or ways of preventing this erroneous falling edge would be appreciated.

Jack