How to interface IDT70V28 HIGH-SPEED 3.3V 64K x 16 DUAL-PORT STATIC RAM on verdin-imx8mp custom base board

Hello All,

I am very new to this DPRAM , i have requirement of porting the DPRAM on verdin-imx8mp using yocto build, Can anyone provide me the useful information to interface DPRAM in yocto.

Thanks in advance.

Parents Reply
  • 1) Renesas do not know anything about the host device

    2) Renesas do not know how the memory is hooked

    3) Renesas do not know where the memory is mapped

    4) Renesas do not know anything about the SW running on the host device

    And Renesas is supposed to provide sample code? Could you explain why?

    It's a memory: you provide the address and you get / write data into it, the "code" can be as simple as a SINGLE load / store instruction.

Children
No Data