Hello team,we have connected dpram to the verdin base board through the gpio pins which are free to use. we have connected D0 to D7 data pins and A0 A15 pins. we want to perform write and read operations. Can you please provide me the any sample code (like to wrire the data continously to the three or more address and after have to those data.)Thanks in Advance,
surya.
Hi Surya,Thank you for posting your question online and apologies for the delay.
surya said:Can you please provide me the any sample code (like to wrire the data continously to the three or more address and after have to those data.)
Unfortunately, we do not provide any sample code or drivers for our Memory products.Please refer on 70V28 - 64K x 16 3.3V Dual-Port RAM | Renesas for all the available documentation. Best Regards,OV_Renesas