multiple relative humidity sensors

Hello,
I would like to exchange DS18B20 sensors ligned up on pcb probe by humidity and temperature sensor.
Could you please help to solve that:
-1 every sensor coupled to the common bus line should have its own resistor?
- 2 40cm distance on PCD is ok, or what thickness on PCB is recommendet?
- 3 acquiring data for every of the attached sensor is possible one after the other?
- 4 is atiming of a raspberry pi zero sufficient?
- 5 is sample code in python available?
many thanks
best regards

Parents Reply Children