Hi,
one of our new devices is designed with the FS2012 flow sensor, and now that we are moving it to production we find it is "Not recommended for new designs"
Thats very very unfortunate, our products usually have a "sales lifetime" of 10 years, and we support them much longer.
The obvious question is: what could replace this sensor? We measure up to 2 liters / minute of air, at max pressure of 1.4 bar.
I have searched the Renesas catalog but nothing even comes close.
Richard