I wrote I connect script that does exactly what the script in log file created and initialization of the ZSSC3281.
The difference is the that the ZSSC3281 kit turn all the 4 LEDs on the ZSSCSRBV3 board (5V,12V,KS5V and KS12v) and my script turn on only 3 LEDs, and not the KS12V LED.
That is missing in the script?
What the KS5V and KS12V LEDs role in the board?
Elik