ZSC31050

Hello! I have some questions about ZSC31050. Firstly, I hope you can provide me with the DLL files of ZSC31050 to suppor me design. Secondly, I had brought the ZSC31050 SSC Evaluation Kit form taobao. But when I choose IIC--COMM--BOARD, there are some mistakes happen: 1. It seems, activating of command mode (CM) failedor transmission speed is to fast! Power off the $sC and execute start procedure again orreduce tramsmission speed in -dialog! Communication error detected, error code = 032. 2. I check the voltage of the Comm board, only 5P and 12P has correctly voltage, other pin(KS5V、KS12V、VPP、VDD-LS、KS-LS) is zero,the voltage of SSC Board ZSC31050's VDDA pin is zero, could you tell me what should I do? 3.In the section 5.3 of ZSC31050 Functional Description, the default value of Configuration Word CFGSIF SIFOUTP=1; SIFOUTT1=1, how to relaize the readout of them? (if we want to the value of T1,Ijust set SIFOUTT1=1, SIFOUTP=0) 4.In the section 2.3.3 of ZSC3105 Datasheet , I want to know the meaning of Measurement count n and the different about it.