Dear,
good day!
we use ZSC31015 as piezoresistive bridge sensor signal conditioning to assemble pressure sensor. Everything runs smoothly. We meet strange thing that when we put the pressure sensor into use, if we add 100nF to 470nF capacitor at sensor output PIN to the ground to smooth the signal, about 2% products would occur Oscillation in output. The frequency is 42.117kHz and amptitude is 400 mVpp. if we remove the capactor, the output signal is fine.
why this phenomenon happen? could you list some factors caused this issue?
Many thanks and Best Regards,
Jarvis