ZMOD4410 testing conditions and environment compensation

dear team,

thanks for a promising product so far.

my goal is to determine human presence in the room using co2 as a proxy. This is why i'm interested in the eCO2 from ZMOD 4410.
I Understand the gas sensor is not an NDIR CO2 sensor and will not measure actual CO2, yet I'd hope it would be close enough.

I've been running 3.2.0 library and sensor is providing results.

unfortunately the figures do not seem to correlate with human presence in the room. I know that there will be a delay of at least 15-30 min for the sensor to react.
sensor is running for more than 48h
so this is why I'd need your help.
Please find a few hints about the setup so far.

Is there a testing procedure to ensure that sensor is actually ok,
It would be very helpful for you to share a test procedure to confirm that readings in specific test conditions are correct:
for example controlled conditions can be based on salt and ethanol concentration in containers.
This would help understand whether the sensor is working correctly and we can compare results with factory results.

secondly, I understand there is temperature compensation if we provide temperature.
Can you help us understand how important temperature compensation is, especially if variation is 'small' in the ambient air , e.g.  between 23 and 28 deg.

finally, I see there is new firmware 4.2.0.
I have still rouble to upgrade, but can you indicate if v4.2.0. will be substiantially better at evaluating e-c02 ?
based on release notes, it seems there is no major improvement with v4.2.0.

Thanks again for your help as sensor seems very promising.