Dear Support,
I would like to use the IPS2550 in Single-ended mode.
In Table 2 of the datasheet, I see that pin 13 (SINN) and pin 11 (COSN) are renamed "REF," and represent the VDD/2 reference.
Can I connect both pins 13 and 11 together on my design?
Thank you in advance for your help.
Best regards.
Hello clochu ,
Thanks for reaching out Renesas Engineering Community.
Please let me check this internally and I will get back to you.
Thanks and Regards,
IK
Our recommendation is to leave pins 13 and 11 floating.