5P49V6965 Phase Shift Won't Exceed 110 degrees

Hello I am working with the 5P49V6965 on a custom devboard as well as the 5P49V6965-EVB.

I am having trouble getting any of the outputs to have more than 110 degrees phase shift from each other.
The Timing Commander software allows me to set higher values but after 110 degrees the actual values at the output are no longer accurate.

I also tried doing my own calculation based on the "Register Descriptions and Programming Guide" which produced the same values as the Timing Commander software.
Confusingly, the values calculated in the data sheet don't seem to be correct? (2 ^ 6) = ***.  *** * 0.82 = 52.48, 52 = 34 (hex)


The following is my configuration on the EVB generated by the Timing Commander software.

Parents Reply Children
  • Former Member
    +1 Former Member in reply to MasonM

    MasonM,

    Yes, you’re right based on design team suggestion we will overflow register. But thanks to a member of the engineer team : provided temporary solution. By programming OD4 integer value to 2112(R0x5B = 0x84, R0x5C =0) for 396.4kHz. We got phase shift around ~135 degree with output 1 as the reference, you can try this work around solution.