Hello,
I am new to use Renesas MCU.
How can I setup device drivers and MCAL for X5H ?
I installed E2 Studio but could not find an option to add the packages for X5H
Best regards,
Nandan Chaturbhuj
Can you give more details about X5H device ? I do not think there is such Renesas MCU.
https://github.com/renesas-rcar/meta-renesas/blob/dunfell/meta-rcar-gen5/conf/machine/x5h.conf
Please check this device.
Possibly also called r8a779g0
Hello Nandan Chaturbhuj,
Thank you for sharing information.Unfortunately, this question cannot be dealt with in this group/fourum. ----------------------------------------------------------------------------------------------This group and the forums it contains cover the following only: - R-Car S4 Whitebox SDK- Linux BSP and Xen(Hypervisor) for R-Car S4 Starter Kit board----------------------------------------------------------------------------------------------
And X5H information isn't published.So I will close this ticket. If you can post question without non-public information, please submit new question.