2.If the answer to the first question is affirmative, then I encounter the following issues:
I want to implement a test project to measure the network speed of CR52. So, I modified the "ethernet" example in the Whitebox SDK , and added lwiperf. However, the lwiperf implemented by default in the Whitebox SDK for CR52 is extremely slow. I tried modifying the RSWITCH_MAX_NUM_CHAINS in rswitch.c for experimentation. Although the network speed increased, it still remains very slow. Could you please advise on how to improve the network speed to achieve a level closer to normal speed (on CR52)? Attached are the results of the experiment:
*Linux←→Linux(control group)
*
exp1: Default WhiteBoxSDK Linux←→CR52 lwiperf very slow
exp 2: Increasing the value of TX_RX_RING_SIZE in Rswitch.c improves the speed of the network.
#define TX_RX_RING_SIZE 1024
exp4: Modifying the network's window size yields unreasonable data.
exp 5: Continue to increase TX_RX_RING_SIZE 2560
CR52 fw crash