I am using safegauto within Whitebox.
GitHub - renesas-rcar/whitebox-sdk: R-Car S4 Whitebox SDK repository
safegauto is from Commits on August 20, 2024.
I am experimenting with it on Spider.
In safegauto, the Makefile.config contains the following:
ifeq ($(TARGET), renesas_rcar_s4)
RLIN3_PORT0 = 7
….
endif
Additionally, in \hypervisor\obj\obj_1pe_atk2\sample1.c, there is:
syslog("HV%d : RH850v2 HyperVisor start on Core%d!\n", coreid, coreid);
The syslog is output through RLIN3_PORT0, which corresponds to LIN7, so there should be a waveform.
However, when measuring CN38[58] RLIN37TX with an oscilloscope, no waveform is detected.
Could you please help identify what might be the issue?