Hello Renesas,
While researching, I learned that the S4 board includes an integrated 12-bit SAR ADC, which can monitor external signals and help track hardware lifespan. Based on this, I would like to know which sensors are embedded in the S4 board itself, specifically excluding network-related sensors.
Thank you.
Hi,
Sorry I don't really get your question. But if you want to know which components, interface can be used on the board, please check the hardware manual:
- S4 Starter Kit: Y-ASK-RCAR-S4-1000BASE-T - R-Car S4 Starter Kit | Renesas
- S4 Spider: RTP8A779F0ASKB0SP2S - R-Car S4 Development Board/Spider | Renesas
Could you tell me which sensor or peripheral that you are looking for?
Hello,
Thank you for the information!
My question was about any built-in sensors that come pre-installed on the S4 board itself, excluding any network-related sensors. Specifically, I am interested in knowing if the board has integrated sensors for monitoring parameters like temperature, humidity, or voltage—anything that could work with the 12-bit SAR ADC for tracking hardware lifespan, reliability, or environmental conditions.
Thank you again for your help, and I appreciate any insights on this!
S4 board does not have such kind of sensors that you mentioned. S4 was designed for car servers and communication gateway. Therefore, you can find only communication interfaces.
The 12-bit SAR ADC is actually the ADC on PMIC (RAA271005), and we don't provide software to use it.
Best Regards,
Duy Dang
Hi Shubham,
More than 2 weeks have passed since this ticket was last updated. If this topic will be discussed continuously, please update it. If there is no update by 12/16, it will be automatically closed.If you have any updates or want to ask another question, please post new question.