i have inserted a nano sim card on kingfisher board and tried call but could call is not connecting (operator saying switch off)
Hello Aditya_Chawla,
KF BSP doesn't support sim.
See below for supported functions.
https://elinux.org/R-Car/Boards/Kingfisher/Yocto-Gen3/v5.9.0#S.2FW_support_status
Hi:
I'd like to clarify for detail information:
[1] Hardware setup: Which model of starterkit + kingfisher board you are using? (e.g. H3 Starterkit + Kingfisher)
[2] Software version: Which software you are using? (e.g. Linux or Android, which version)
Hardware setup : H3 SK + KF
Software setup : Linux