How to use COMExpress on Rcar H3 with Kingfisher Infotainment Board?

Hello all,

I have connected Kingfisher infotainment board with Rcar H3 Starter Kit using the COMExpress. I want to know how i can make use of the HW capabilities of the Kingfisher Infotainment board through the COMExpress. Are there are specific steps that need to be followed to enable the COMExpress? 

For eg: If i want to use the HDMI port available on the Kingfisher Infotainment board then what are the things that need to be done?

Thanks, 

Pinakin Brahmin

Parents Reply Children
No Data