Hello Community First message, will try to follow the rules
Reading this https://community.renesas.com/automotive/r-car-h3-m3-cockpit/f/cockpit-f/17652/android-9-or-android-10-with-dual-multi-display-display-support-som
I'm happy to run the H3 with 2 dislplays, and able to start an activity via adb on the second display.But I didn't find anyway to get a working mouse (or any other input) on the second display.Seems that even google doesn't support this in AOSP 9: https://source.android.com/docs/core/display/multi_display/input-routing
Obviously I have to keep Android 9 (else would switch to 10 :) )Any solution ? Feedback?Many thanksVincent
Hi Vincent:
Confirmed with engineer but they also said in Android 9 and lower, there was no way to interact with multiple displays via touch, because there was no association mechanism between displays…
Confirmed with engineer but they also said in Android 9 and lower, there was no way to interact with multiple displays via touch, because there was no association mechanism between displays and input devices. (as you searched the explanation https://source.android.com/docs/core/display/multi_display/input-routing)
Hello Vincent,
Do you have any update?
This question has been opened but there is no reply for a long time.
We have a tentative answer already, so I will close this question.
If you have any updates or want to ask another question, please post new question.