Hii
Specifications:—
Hardware Platform : Renesas r-car H3e skGPU Device : PowerVR Series6XT, GX6650
Is GX6650 GPU support vulkan or not?
Hello Sumit,
The GFX package for Linux Yocto BSP doesn't support Vulkan.It supports only OpenGLES.Also, you cannot run HW(GPU) without using GFX package.
https://www.renesas.com/us/en/application/automotive/r-car-h3-m3-h2-m2-e2-documents-software
FYI:Yocto Linux BSP v5.9.0 eLinux site for R-Car H3e/M3 Starter Kithttps://elinux.org/R-Car/Boards…
Hi gohda,
Can you give GFX package link which you have used?
FYI:Yocto Linux BSP v5.9.0 eLinux site for R-Car H3e/M3 Starter Kithttps://elinux.org/R-Car/Boards/Yocto-Gen3/v5.9.0
Hello Gohda,
Is the same GFX package used for Debian Linux?
Can you give me the steps to integrate the GFX package on Debian Linux?