LVDS on Kingfisher Infotainment Board

We are using R-Car h3 Starter kit + kingfisher Infotainment Board and i want to use LVDS out port in kingfisher infotainment board. But, i am not able find a convertor for LVDS out port which flat panel 20 pin port

I have attached image of the LVDS flat panel port.

I need to buy LVDS to HDMI convertor for Kingfisher Infotainment Board because im using lilliput display which only supports HDMI input

Can someone help me with a link from where i can buy the LVDS to HDMI convertort with 20 pin cable in india.