Hi
Platform Specification: -
Hardware Platform:- RTP8J779M1ASKBOSK... Renesas R-Car h3
Operating System(Host): - 20.04.1-Ubuntu x86_64
While compiling and flashing images after completed Yocto build according to https://elinux.org/R-Car/Boards/Yocto-Gen3/v5.9.0, there is an error
Error:-
U-Boot 2020.10 (Jul 20 2022 - 02:42:29 +0000)CPU: Renesas Electronics R8A7795 rev 3.0Model: Renesas H3ULCB board based on r8a77950DRAM: 7.9 GiBRAM Configuration:Bank #0: 0x048000000 - 0x0bfffffff, 1.9 GiBBank #1: 0x500000000 - 0x57fffffff, 2 GiBBank #2: 0x600000000 - 0x67fffffff, 2 GiBBank #3: 0x700000000 - 0x77fffffff, 2 GiBMMC: sd@ee100000: 0, sd@ee140000: 1Loading Environment from MMC... OKIn: serial@e6e88000Out: serial@e6e88000Err: serial@e6e88000Net: eth0: ethernet@e6800000Hit any key to stop autoboot: 0 Failed to load '/boot/Image'Failed to load '/boot/r8a779m1-ulcb.dtb'Bad Linux ARM64 Image magic!
Are there errors in images while compiling or is there an error in settings in uboot etc. ?
Thank you.
Mr. Gohda,Thank you for your reply.There was a problem while mounting and copying the image files to SD card and the SD card was empty. I reformatted and flashed again. The kernel booting completed normally…