Hello,
I am working on RCar-E2-SILK board,Rev1.0 for one of our Requirements.
I am facing issue in Yocto Build Set Up.I am following below links for set up
https://elinux.org/R-Car/Boards/Yocto#Ubuntu_and_Debian
https://elinux.org/R-Car/Boards/SILK#Build_Yocto_image
Below is the Screenshot of my Errors after i give the command bitbake core-image-weston
I am using Ubuntu-20.04 version for build.What is the recommended Ubuntu version for the build?
Queries:
1.Is there Still Support for RCAR- E2 Silk Board ?if there is ,where can i find updated documents to set up Yocto and also to boot from SD card/Flash?
2.Is it Recommended to move forward with Rcar-e2 Silk board?
As per my requirement i need to work on DDR3 configuration specifically on RCAR-E2 Silk Evaluation Board
Regards,
Sanath