E0562330:Relocation size overflow

Hope can find solutions here.

1. I have a code like this:

----------------------------------------------------

#pragma section text "RAMCODE"

void ram_function(){

}

----------------------------------------------------

2. and this is my link setting:

----------------------------------------------------

-START=RAMCODE.text/00017000
-START=RAMCODE.text.R/FEBF8000


-ROM=RAMCODE.text=RAMCODE.text.R

----------------------------------------------------

3 Last, There is another code that invoke ram_function()

main.c

----------------------------------------------------

int main(){

     ram_function() /* This line is OFFSET "00000005" on main.prn */

}

----------------------------------------------------

and I got error like this

E0562330:Relocation size overflow : "obj\Appl\Source\main.o"-".text"-"00000005"

I use RH850-F1KM-S1, am I missing something here?

Parents Reply Children