Bootloader and Application Project Development for RH850

 I need an example code for the development of the bootloader and application project for rh850.
To give a summary, I require to develop a bootloader that can facilitate the flashing of application code via CAN (UDS).
Since I am new to RH850, I am not sure how to set the linker files, alternative Interrupt vector table, trigger reset, and jump to the app from the boot and vice versa.
I need an example code/document for a head start on this.

Parents
  • I have a some questions in interrupt vector table. can you please explain?

    In my controller i changed memory location from starting vector address of 0x00 to 0x8000. In my question is I need vector table address also located in 0x8000 , How to remapped vector table address? and if any changes in vector table address any possible to affected in flash memory lifetime.

Reply
  • I have a some questions in interrupt vector table. can you please explain?

    In my controller i changed memory location from starting vector address of 0x00 to 0x8000. In my question is I need vector table address also located in 0x8000 , How to remapped vector table address? and if any changes in vector table address any possible to affected in flash memory lifetime.

Children
No Data