RH850:How to use the hot plug function of e² studio? Renesas e² studio Version: 2022-10 (22.10.0)

I encountered a problem when using the hot plug function, as shown in the picture below. Does anyone know the reason? How to solve it? Thank you so much!

I set the hot plug to YES

Then I connected the debugger to the target board and hit OK.The problem in the image below occurs.

Does anyone know why that is? Is there a problem with my debug configuration or something? Thank you very much.

Parents Reply Children