Can I control BLDC of 12V and 40amps Motor using RH850 starter Kit? If so, can I connect it to the Non contact torque sensor?
I suppose that question is for the F1KM-S1 starter kit, not F1KH-D8.
No, this is not possible. There are current measurement shunts on the board, which would be damaged by 40A current.
Thank you for your reply. But can I operate 40amps motor with F1KM-S1 starter kit that you mentioned?
No, this is not possible.The current measurement shunt is 0.01 Ohm, 3W. This limits the current to about 17.5A. At this current, the shunt will melt and burn.Actually I don't see a starter kit for 40A motors in the Renesas portfolio.