Dear,
im using lauterbach(trace32) debugging RH850/U2A16/R7F7.
Two questions are blocking
1. if the csa is configrured as double map mode, my tools could only reprogram my code to the un-active bank..
a. for example, if the active bank is B, my tools could only reflash my hex file to the A bank(according to the absolute address in hex or elf file)
b. how could i reprogramm my compiling result to the active bank?
2. how could i use trace32+lauterbach to reprogramm the csa area?
a. my srcipt.cmm is as below step
system.reset
system.config.debugprottype csi
map.reset
system.mode prepare ;; this command will always report ERROR!
flash.reset
b. my t32 will report error after the ''system.mode prepare'' command, reading---"ERROR: System.coreclock setting out of range (800000)"
Have a look at the script "rh850_serialflashprog.cmm" in the latest RH850/U2A script package on the Lauterbach web site under Downloads->Start-UP and other Scripts:
; --------------------------------------------------------------------------------; @Title: Setup for RH850/U2A SerialFlashProgramming (R7F702Z19EDBG); @Description:; SerialFlashProgramming allows programming of:; - all CPU Flash-areas and; - programming of the OptionBytes; - script supports DoubleMap- and SingelMap-Mode;; @Author: STA; @Board: RH850-U2A-516PIN-T1-V1; @Chip: R7F702Z19EDBG; @Copyright: (C) 1989-2021 Lauterbach GmbH, licensed for use with TRACE32(R) only; --------------------------------------------------------------------------------; $Id: rh850_serialflashprog.cmm 17359 2021-03-19 08:43:01Z estahleder $