Can't erase the block of code because of lock bit

I download the application using flash downloader ftool. At this time, lock bit is not set.

But a lock bit of special block is set when Bootloader try to erase the block of code for application.

So Bootloader can't received the response of erase command because of lock bit.

What should I do to resolve this issue?

Parents Reply Children