Hello Sir,
Requesting a solution for periodic updating value of variable in watch register. Configuring it looks different than RL78 .I am using
IDE - CS+
MCU - RH850/FIKM-S1 (R7F701686) 100pin
Emulator - E1
Hereby i have screenshot of the same.
Thanks & regards.
Hello,
Go to 'Debug Tool Settings' and change the settings to these:
Regards
Yes Sir, i have set this as it is same as in RL78, but still i am unable to see my variable value while configuring adc.
I have configured adc using pot, i need to get value as i rotate it. Here are few screenshot of settings
Here i am blinking LED based on adc value,as i am not able to view those in watch registers.
These LED are always ON.
how shall i proceed...
Thanks and regards.
With the mentioned settings, I just increment a variable in the while loop and I can see it changing values 'real time'.
...