LIN MASTER

how to implement LIN mater sleep mode and wakeup mode?

Parents Reply Children
  • If you use the Smart Configurator, you can configure the wake-up factors and low power modes and use the generated drivers.

    To enter cyclic RUN/STOP mode the device must first enter DeepSTOP mode:

    The mode transition to Cyclic RUN mode from DeepSTOP mode is triggered by wake-up factor
    2, and the mode transition to Cyclic RUN mode from Cyclic STOP mode is triggered by either
    wake-up factor 1 or wake-up factor 2.